Configure the sample FactoryTalk Batch Server
To set up the sample demonstrations for
FactoryTalk® Batch
Material Manager
, configure the FactoryTalk Batch
Server to use the
SampleDemo2
application in the FactoryTalk
Network
Directory. Use the FactoryTalk Administration Console
to configure the FactoryTalk Batch
Server.To configure the sample
FactoryTalk Batch
Server:- OpenFactoryTalk Administration Consoleand sign in to theFactoryTalkNetwork Directory.
- InFactoryTalk Administration ConsoleExplorer, expand theSampleDemo2application. Right-clickSampleDemo2_Serverand selectProperties.
- In theFactoryTalk Batch Services Propertiesdialog, select theGeneraltab.
- In theComputer hosting the primary FactoryTalk Batch Serverbox, enter or browse to the host computer where the primaryFactoryTalk BatchServer resides.
- SelectEnable FactoryTalk Batch Material Manager.
- At the bottom of theGeneraltab go to theMaterial Policiessection. Enter the name of theComputer hosting the FactoryTalk Batch Material Serveror browse to the computer by selecting the
button. - Select theCommunications lost behaviorfrom the dropdown list.
- Select or clear theHold on Split Feedoption.
- SelectApplyto save the data in theGeneraltab.
- IfFactoryTalkis part of your system, do these extra steps:eProcedure
- SelectEnable FactoryTalk eProcedure.
- SelectApplyto save the data in theGeneraltab.
- Select theProject Settingstab.
- In theServerbox, select a server.
- In theServer directoriesarea, for theProject path strategy, selectCustom paths.
- Select theArea Modelbrowse button. TheBrowse for Area Modeldialog opens.
- Open theC:\Users\Public\Documents\Rockwell Automation\Batch\SampleDemo2\Recipesfolder, select theice_cream2ep.cfgfile, and then selectOpen.
- SelectApplyto save the data in theProject Settingstab.
TIP: In order for theServer to start, you must define theeProcedureInstructionspath and have an instruction file for each instruction-based phase in the area model. TheSampleDemo2application automatically populates this path. (See the for instructions on defining instruction-based phases.) - SelectOKto save the data in each tab of theFactoryTalk Batch Services Propertiesdialog and close the dialog.
- Select to exit theFactoryTalk Administration Console.TIP: These steps set up theFactoryTalk BatchServer to run the tutorial steps in this manual. There are many other settings to consider when setting up theFactoryTalk Batchsystem. (See thefor more information on theFactoryTalk Batch Administrator's User Manual, publicationBATCH-UM003FactoryTalk Batch Services Propertiesdialog.)
Provide Feedback