Configure the Network Editor
Configure the Material Server with the location of the SQL database that contains the
materials for the SampleDemo2 recipes.
- Select , and selectNetwork Editor.
- In theNetwork Editorwindow select the Material Server.TIP: This procedure requires administrator privileges.
- SelectConfigure. TheConfigure FactoryTalk Batch Material Managerdialog opens.
- In theMaterial Databasebox, enterSAMPLE2_MATERIALS, and selectOK.
- To exit the Network Editor, select , and clickYes
Provide Feedback