Browsing devices

When
ControlFLASH Plus
is started for the first time, the
Browsing from path
is not configured. You need to configure the browsing path in the
Network Browser
. After you set the path for the first time,
ControlFLASH Plus
will use the last selected path setting.
Once a starting browse path is configured,
ControlFLASH Plus
uses the configured browsing path and number of levels to populate the devices list. The devices are shown with the current versions of firmware and available compatible firmware revisions are shown in the
Flash To
column. The topology is refreshed when opening
ControlFLASH Plus
or changing the browsing path in the
Network Browser
.
When updating topology and devices, you may cancel progress by clicking the
Cancel
button. Clicking the
Cancel
button opens the
Network Browser
for you to select another
Browsing from path
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal