Generating the devices list
The devices list is generated differently depending on what is chosen as the starting node.
When a device (for example 1756-L85E) is selected, only the device itself is shown in the devices list.
TIP:
A bridge node is also treated as a device node, for example, 1756-ENBT/A.
When a bus is selected, such as a backplane ("1756-A10/A"), a network ("Ethernet"), or a
FactoryTalk Linx
driver ("AB_ETH-2"), all items under the bus, up to the number of levels configured, are shown in the devices list.Provide Feedback