Browse path and levels

Clicking FT Linx on the
Flash Devices
tab opens the
Network Browser
. Use this dialog box to select a node in the
Network Browser
tree as a starting point for browsing devices. Clicking
OK
refreshes the device list on the
Flash Devices
tab.
The dialog box allows you to choose the number of levels that should be browsed. The maximum number of levels to browse is 3. The default value of levels to browse is 2. Selecting a device as the starting point will ignore browse levels and only browse that device. The performance of detecting devices may be impacted if FactoryTalk Linx provides this warning. The way to avoid this warning is to reduce the number of IP addresses that are being browsed.
Network browser warning
IMPORTANT:
In the
Network Browser
, you must expand each level of the node that includes the devices you need and wait until all the devices are detected.
When selecting the root node in the
Network Browser
tree,
OK
is disabled by default.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal