Overview view

In the
Device Definition
dialog, use the
Overview
view to:
  • Enter the name and description for the device.
  • Enter the IP configuration for the device.
  • Define the series and revision of the device.
  • Select the electronic keying.
  • Configure the connection and data formats.
TIP:
  • The parameters in this dialog appear shaded in Run mode.
  • While online, the only editable parameters are
    Description
    ,
    Electronic Keying
    , and
    IO-Link Class B Enabled
    .
  • After making a change and selecting
    OK
    in the
    Device Definition
    dialog, you must select
    OK
    or
    Apply
    in the
    Overview
    view for the change to take effect.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal