Rename an axis

Use the following steps to rename an axis.
To rename an axis
  1. In
    Project Organizer
    , double-click the controller node to open the controller application workspace.
  2. In the
    Controller
    tree, under
    PTO Motion
    , select
    Axis<x>
    .
  3. On the
    Axis<x> - General
    configuration page, in the
    Axis name
    box, enter the new name.
    TIP: To delete an axis, on the PTO Motion - General configuration page, clear the
    Axis<x>
    checkbox.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal