Add an axis to the controller project
For
Micro800
controllers that support motion control, the PTO Motion
node is available in the Controller
tree.To support motion control in a
Micro800
controller project, you must add an axis to the controller project and configure motion control settings on the Axis<x>
configuration page. The number of supported axes depends on the controller type.After adding an axis to the controller project, in the
Controller
tree, under the PTO Motion
node, an Axis<x>
node is created. Selecting the Axis<x>
node opens the Axis<x>
configuration page, which contains the following pages:To add an axis to the controller project
- InProject Organizer, double-click the controller node to open the controller application workspace.
- In theControllertree, under thePTO Motionnode, selectGeneral.
- On thePTO Motion - Generalconfiguration page, select the axis you want to add.Upon selecting, theAxis<x>nodes are created underGeneralin theControllertree.
Provide Feedback