Import Export Template Manager
How do I open the Template Manager?
- ClickTOOLS > Import Export Manager.
- InImport Export Manager, clickTOOLS > Import Export Template Editor.
The
Template Manager
can be used to create custom schedule templates, copy schedule templates, or move schedule templates from one location to another.Three schedule template locations are available:
- Local: In the Windows User Folder. Available only to the ACM User.
- Project: In the ACM database. Available to all ACM users with this project currently open.
- Global: In the ACM database. Available to all ACM users connected to this ACM database.
Provide Feedback