Create a schedule template
Use the
Template Manager
tool of the Import Export Manager
to create schedule templates. Schedule templates determine the scope of the schedule (local, project, or global), the library objects used, and the parameters that are visible.To create a schedule template
- ClickTOOLS > Import Export Manager.
- InImport Export Manager, clickTOOLS > Import Export Template Editor.TheTemplate Managerappears with theTemplate Editortab displayed.
- In theTemplatearea, make the following selections:
- Select the scope of the template:
- Local
- Project
- Global
- (if project scoped) Click the down arrow and select the project name.
- Click the down arrow and select the schedule template.
- ClickNew. TheTemplate Namedialog appears.
- InNew Template Name, enter a name for the new schedule template and clickOK.The new schedule template name appears in theTemplatearea.
- In theLibrary Section Selectionarea, add the object and subobject parameters to the new schedule template.
- Select an object in theLibrary Section Selectionarea.
- In theNot Visible Parametersarea, select the parameters to include.ClickSelect Allto select all of the parameters for an object.
- ClickAdd >.
- Repeat as needed.
- In theVisible Parametersarea, order the parameters as they should appear in the template file.
- ClickSaveto save the changes.
- ClickReloadto cancel all edits made since the last time theSavecommand was executed.
- ClickFinishto close theTemplate Manager.
Provide Feedback