Reports

Application Code Manager
includes a variety of reports to help you track the usage of code objects in your projects.
This table lists the reports available:
Report
Description
Project History
For the current project, shows the major revision, minor revision, the user account that made the revision, the date and time that the revision occurred, the comment associated with the revision, and the status of the project at the revision point.
All Library Usage (Current Project)
For the current project, shows the name of the solution, the type of library, the category of the library object, the catalog number of the library object, the major revision of the library, the minor revision of the library, the number of usages of the library object in the project, and the status of the library.
Library Usage per Solution (Current Project)
For the selected library in the current project, shows the type of library, the category of the library object, the catalog number of the library object, the major revision of the library, the minor revision of the library, the number of usages of the library object in the solution, and the status of the library.
Library Usage per Library Type (Current Project)
For the selected library type in the current library of the current project, shows the category of the library object, the catalog number of the library object, the major revision of the library, the minor revision of the library, the number of usages of the library object in the solution, and the status of the library.
Library Usage per Category (Current Project)
For the selected category in the selected library type of the current library associated with the current project, shows the catalog number of the library object, the major revision of the library, the minor revision of the library, the number of usages of the library object in the solution, and the status of the library.
Library Usage for Selected Library (Current Project)
For the selected library object within a selected category in the selected library type of the current library associated with the current project, shows the total number of times the library object is referenced and the number of times the object is used by each controller in the current project.
Chassis Layout
For the chassis of the selected controller object, shows the slot assignments, module names, module type, and module information.
I/O Schedule
For the selected I/O module of the current controller object, shows the I/O points, type, module information, and description.
Network Layout
For the selected communication module of the current controller object, shows the IP address assigned to the module, the module name, the module type, and connections information.
Library Usage per Project
For the connected ACM database, shows the solution, the library type, the library category, the catalog number, the major revision, the minor revision and the number of times used in projects.
Pending Libraries in database
For the connected ACM database, shows the libraries that have not yet been published. Identifying them by solution, library type, category, catalog number, major revision and minor revision.
Library Usage per Solution in database
For the selected solution in the connected ACM database, shows the library type, the library category, the catalog number, the major revision, the minor revision and the number of times used in projects.
Pending Libraries per Solution in database
For the selected solution in the connected ACM database, shows the libraries that have not yet been published. Identifying them by library type, category, catalog number, major revision and minor revision.
Library Usage per Library Type in database
For the selected library type of a solution in the connected ACM database, shows the library category, the catalog number, the major revision, the minor revision and the number of times used in projects.
Pending Libraries per Library Type in database
For the selected library type of a solution in the connected ACM database, shows the libraries that have not yet been published. Identifying them by category, catalog number, major revision and minor revision.
Library Usage for Selected Library in database
For the selected library object within a library type, shows the total number of times the object is used and the usages per project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal