Generate a report
Reports are generated from the
View
context menu. Different reports are available depending on the object selected.To generate a report
- Select the object in the tree that you want to report on. Reports are available from objects in the System View, Preview, Class View, and Registered Libraries panes.
- Right-click the object, selectViewand then choose the report to run.
- The report appears in a new window.
- If there are multiple pages in the report, use the navigation controls to move forwards and backwards through the report information.
- To rerun the report to incorporate changed information, clickRefresh.
- To send the report to a printer, clickPrint.ThePrintdialog opens. Confirm that the printer inSelect Printeris correct. Optionally, specify thePage RangeandNumber of copiesto print. By default one copy of all pages in the report are printed. ClickPrintto print the report.
- To save the report to a file, clickExportand then chooseExport to Word,Export to Excel, orExport to Pdf.TheSave Asdialog opens. InFile name, type a name for the report being exported.Save as typeis already selected for the appropriate file format (.pdf, .xlsx, or .docx).ClickSaveto save the report.
Provide Feedback