Console scripts
A console script is a text file (.txt) containing a set of valid
Application Code Manager
Console commands. The commands are run in order, top to bottom.If using the CREATEPROJECT, CREATECONTROLLER, or CREATEOBJECTS commands, the console script requires an Extended script (.xml) file. The Extended script is called as part of the command to provide data to
Application Code Manager
about the project, controller, or object that is created.Provide Feedback