Create an ACM Console script

Create an
Application Code Manager
Console script to store a set of commands for later or repeated use.
To create an
Application Code Manager
Console script
  1. Open a text editor, such as Notepad.
  2. Enter one or more valid
    Application Code Manager
    Console commands into the script.
    IMPORTANT:
    Only enter one
    Application Code Manager
    Console command per line of the script.
  3. Save the script as a plaintext (.txt) file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal