Run an ACM Console script

Run an
Application Code Manager
Console script to execute a set of predefined commands on the
Application Code Manager
database.
To run an
Application Code Manager
Console script
  1. Double-click the
    ACM Console
    shortcut on the desktop.
  2. Select
    File > Run Script
    .
  3. In
    Select an ACM Script File
    , locate the file, then click
    Open
    .
    The script executes.
Alternatively:
  • At the
    Application Code Manager
    Console prompt, type
    run path\scriptfilename.txt
    , then press
    Enter
    .
    Replace
    path
    with the file path, such as
    C:\Users\<username>\Desktop\
    and
    scriptfilename.txt
    with the script filename.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal