OPCItems collection
The OPCItems collection is an automation collection that contains all of the OPCItem objects this client has created within the scope of the OPCServer, and corresponding OPCGroup object that the Automation Application has created. The following properties and methods are included in the OPCItems collection:
Properties
Methods
Provide Feedback