OPCItem object
The OPCItem object is an automation object that maintains the item's definition, current value, status information, and last update time. Note that the Custom Interface does not provide a separate Item Object. The following properties and methods are included in the OPCItem object:
Properties
Methods
Provide Feedback