DefaultAccessPath property

Description
(Read/Write) The default AccessPath that will be used when adding items. This property defaults to "".
Syntax
DefaultAccessPath
As String
Example
'/* Set the default access path
MyOPCGroup.OPCItems.DefaultAccessPath = "MyTopic"
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal