Remote Routing Configuration

The options in the
Remote Routing Configuration
dialog box vary, depending on the current communication hardware driver and the bridge device selected.
Bridge Device list
RSLinx Classic supports six different methods (listed in the
Bridge Device
list) for accessing remote processor networks:
The
Remote Routing Details
portion of the
Remote Routing Configuration
dialog box varies, depending on which of the previously defined remote routing methods is selected in the Bridge Device list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal