Ethernet EI RM Module Bridge Device
Use the Ethernet EI RM Module bridge device setting to communicate to a remote DH+ through a PLC-5/250 Resource Manager from local Ethernet. When the Ethernet EI RM Module bridge device setting is selected, the
Remote Routing Configuration
screen opens.Provide Feedback