Add modules to the routing table

To add a module to the routing table:
  1. In the 1756-DHRIO interface, select the
    Routing Table
    –
    Configuration
    tab.
  2. Select the backplane or link to which you want to add the module.
  3. Right-click and select
    Add Module
    .
  4. In the
    Select Module
    dialog box, select the module type for the module you want to add.
  5. Click
    OK
    .
  6. Select from the following table:
    Adding a module to:
    Do this:
    The controlLogix backplane
    In
    Slot Number
    ,
    of the
    Add Module
    dialog box, enter a slot number. Valid values are 0-19 (decimal). The ControlLogix system begins slot numbering at 0.
    A ControlNet link
    In
    Network Address
    ,
    of the
    Add Module
    dialog box enter a network address. Valid values are 0-99 (decimal).
    An Ethernet link
    In
    IP Address
    , of the
    Add Module
    dialog box, enter an IP address. Valid values are xxx.xxx.xxx.xxx where xxx is a number from 0-255 (decimal).
    A DH+ link
    In
    Station Address
    , of the
    Add Module
    dialog box, enter a station address. Valid values are 0-77 (octal).
  7. In
    port link ID
    of the
    Add Module
    dialog box, enter any link IDs of the link on the other side of the module. Valid values are 1-199 (decimal).
  8. Click
    OK
    .
    TIP:
    If you do not want to assign a link ID, enter
    0
    . DH+ bridge modules allow a list of link IDs to be entered. Link IDs are all the links that can be reached through that bridge. Workstations can have a link ID that is used to deliver unsolicited requests to applications on that workstation, where each application has its own station address.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal