Configure a RAS server
- In Windows NT Explorer, right-click theNetwork Neighborhoodicon and selectProperties.
- Under theServicestab, make sureRemote Access ServiceandSimple TCP/IP Serviceappear. If they do not appear, clickAdd, and select each of them from the list, and clickOK.
- SelectRemote Access Serviceand clickPropertiesto display theRemote Access Setupwindow.
- Select the appropriate RAS device. If no RAS device is available, clickAddand configure the device.
- ClickConfigureand selectDial out and Receive Calls.
- Return to theRemote Access Setupwindow and clickNetwork.
- For Dial out Protocols and Server Settings, selectTCP/IPand click Configure.TIP:If a DHCP server is not available, a range of IP addresses can be given to a RAS server for assignment to clients. The range must be valid for the subnet the RAS server is in. Type the beginning and ending addresses of the range in the appropriate box. You must assign at least two IP addresses, one for a remote client and one for the network adapter on the RAS server.
- Return to theRemote Access Setupwindow and clickContinue.
- Open the Control Panel and selectServices.
- The following options should be Started and Automatic:
- Remote Access AutoDial Manager
- Remote Access Connection Manager
- Remote Access Service
- Simple TCP/IP Service
- Assign dial in access from Remote Users by clicking theStartmenu and selectingPrograms > Administrative Tools > Remote Access Adminto assign dial in access from Remote Users.
- On theRemote Access Adminon \\computername menu bar, selectUsersandPermissions.
- Select theGrant Dial In Permission to Usercheck box to give the selected user dial in permission. This is the name of the user that will be dialing into the Server machine. You can give everyone permission by clicking theGrant Allcheck box. TheGrant Dial In Permissiondialog box also shows if you are connected by checking the number of ports and active ports.
IMPORTANT:
After configuring RAS server, you must reinstall NT Service Pack 3 for RAS to work. Also, if the server machine does not have a separate network card configured with a valid IP address, you must first install an MS Loopback Adapter and assign it an IP address via TCP/IP protocol.
Provide Feedback