Air Gap automated patch deployment

FactoryTalk Updater v4.10 allows automated air gapped deployment of Monthly Patch Rollups to multiple computers. Communication between these systems is by file transfers. The files require password encryption as they are exported and decryption as they are imported.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal