Import updated Zip file from IT Mode into OT Mode
Once you retrieve the latest software information and patches from PCDC by using IT Mode, import the updated Zip file and patches into OT Mode.
TIP:
To deploy patches and information, the FactoryTalk Updater Client must connect
to FactoryTalk Updater Server with an administrator user account.
- Import the data from the saved.zipfile by selectingUpdate Database.
- Select the exported IT list.
- Enter the password and selectOK.
- Select the products that you want to deploy, and then selectDeploy.
- In theDeploy Patcheswindow, browse for the patch.
- Determine when to install the patch.
- Determine when to restart the computer after installing the patch.
- SelectDEPLOY.
- In theEnter the Credentialdialog box, enter the administrator's username and password of the selected machines, and then selectOK.
Provide Feedback