Patch deployment cancel

Local connection: Use FactoryTalk Updater to collect detailed information for a local network. FactoryTalk Updater provides screens and export to view your software inventory and usage. Another way to consume the data is by connection to the database. With an OBDC driver, connect to the FactoryTalk Updater Server database
C:\ProgramData\Rockwell\Updater\Data\Server.DB
. A workflow to view the Server.DB tables in Excel is shown.
Multiple connections: To scale up beyond a single network or a production line to a production site to a collection of sites, data must be aggregated. Aggregating data from several databases can be accomplished with analytics tools such as Power BI.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal