Delete a graphic object

Delete a graphic object

Delete a graphic object to remove the object from the project. Delete a graphic object from either
Project view
or in the window.
  • In
    Project view
    or in the window, select the container or graphic object and press
    Delete
    .
The object is removed from the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal