- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Compose SQL queries
Filter data using an SQL query to display specific data from the database.
Compose a query:
- As text
NOTE:
You should not specify the table name in the
FROM
clause. Instead, specify the table name in the dynamic link to the BrowseName
of the table with an {0:sql_identifier}
placeholder in a string formatter.Use case: filter by time
Use the
Time
or Timestamp
column that contains the date and time to filter data by time.Use the
sql_literal
literal in the placeholder of the string formatter. Rockwell Automation
recommends using a temporary DateTime
variable.Example. Export records that have a Timestamp greater than a certain instant of time:
SELECT * FROM {0:sql_identifier} WHERE Timestamp > {1:sql_literal}
Example. Export records that have a Timestamp between two instants of time:
SELECT * FROM {0:sql_identifier} WHERE Timestamp BETWEEN {1:sql_literal} AND {2:sql_literal}
TIP:
Use the Timestamp column to create a time filter on a Logger. Use the Time column to filter alarm history.
Use case: filter by alarm severity
The
Severity
column contains the value of the severity of an alarm. Use this column to filter various severities of an alarm grid or alarm history grid.Example. Export the history of alarms with severity 1:
SELECT * FROM {0:sql_identifier} WHERE Severity = 1
Example. Export the history of alarms with severity between 1 and 3:
SELECT * FROM {0:sql_identifier} WHERE Severity BETWEEN 1 AND 3
Use case: filter by alarm or variable
The
ConditionName
column contains the name of the alarm. Filter archived alarms to obtain specific alarms. You can filter alarm names if they follow a specific pattern.The condition can be used on the
SourceName
column to filter by the input variable.Example. Export the alarm history with a given BrowseName in the past:
SELECT * FROM {0:sql_identifier} WHERE ConditionName = {1:sql_literal}
Example. Export the history of the alarms connected to the variable:
SELECT * FROM {0:sql_identifier} WHERE SourceName = {1:sql_literal}
Example. Export the history of alarms starting with Exclusive:
SELECT * FROM {0:sql_identifier} WHERE ConditionName LIKE 'Exclusive%'
Use case: filtering Recorded Alarms
Export some columns of the logger through the
SELECT
statement.Example. Export the alarm history with only the Italian columns:
SELECT "ActiveState_it-IT", "AckedState_it-IT", "ConfirmedState_it-IT", "ConditionName", "EnabledState_it-IT", "SourceName", "Time", "Message_it-IT", "Severity" FROM {0:sql_identifier}
Provide Feedback