IUANode.Get(browsePath)

IUANode.Get(browsePath)

Returns an
IUANode
C# object that corresponds to the first child node of the node on which the method is invoked. The returned object name corresponds to the argument.
IUANode Get(string
browsePath
);

Arguments

browsePath
(string)
Can be either:
  • The
    BrowseName
    of the object
  • The path of the object in the information model, uniquely expressed as a sequence of
    BrowseName
    values separated by
    /

Returns

IUANode
A C# object that matches the requested node.

Examples

The following examples show a returned C# object that corresponds to the
Motor1
node that is a child of
Machine1
:
var motor1 = Owner.Get("Machine1").Get("Motor1");
var motor1 = Owner.Get("Machine1/Motor1");
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal