FactoryTalk Application

How do I open Select
FactoryTalk Directory
?
  • In
    Global Settings
    , under
    Data Source
    , select
    FactoryTalk Application
    , and then select .
Select an application, area, or sub-area (also known as the scope) from the
FactoryTalk Directory
.
The following table shows the supported namespace modes of each server using the
FactoryTalk
Application.
Interface
Folder with scalar data
Tag list and structures/array access
Custom namespace
OPC UA Server
Yes
Yes
Yes
MQTT
No
No
Yes
OPC DA Server
Yes
No
No
RTD Server
Yes
No
Yes
DDE Server
Yes
No
Yes
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal