Configure a FactoryTalk application with a FactoryTalk Linx server
These steps are based on that you are setting up a FactoryTalk application using FactoryTalk Administration Console.
To configure a FactoryTalk application with a FactoryTalk Linx server
- In FactoryTalk Administration Console, add a FactoryTalk Application.
- Add a FactoryTalk Linx server to the application, and then specify the FactoryTalk Linx server properties.
- Open theCommunication Setupeditor, and then add drivers and devices to your network.A driver is the software interface that allows you to communicate with your target hardware device.
- Create a shortcut that point to the device from which you want to obtain data.
- In theDevice Shortcutspane of theCommunication Setupeditor, selectAdd, and then specify the shortcut name.
- From Network Browser, select the target device.
- In theGeneralbox, specify the shortcut properties.Processor, Redundant, Symbolic, EDS Parameter, and CIP Object shortcuts are supported.
- SelectApply.
For more information about setting up an application using FactoryTalk Administration Console, see
FactoryTalk Linx Help
.For more information about setting up an application using FactoryTalk View SE, see
FactoryTalk View SE Help
.Provide Feedback