Linx SDK Interface Installation
The Linx SDK Interface is an optional portion of the FactoryTalk Linx Gateway installation. If you have already installed FactoryTalk Linx Gateway, you can modify the FactoryTalk Linx Gateway installation in the
Control Panel
or from Start > Apps > Apps & Features
. The Linx SDK Interface is installed in:- C:\Windows\System32 for the 32-bit operation system
- C:\Windows\SysWOW64 for the 64-bit operation system
The following files will be installed:
- DTL_ErrorCode.hDefines all error codes returned by the Linx SDK Interface.
- DTLMsgCommon.hDefines the common data structures used in the Linx SDK Interface.
- FTLinx_SDK.dllThe Linx SDK Interface's dynamic link library, which will be used when running the applications.
- FTLinx_SDK.hThe header file that defines all interfaces provided by the Linx SDK Interface.
- FTLinx_SDK.libThe Linx SDK Interface's static library, which will be used when compiling the applications.
Provide Feedback