Linx SDK Interface Activation

The Linx SDK Interface only supports the 32-bit client software. To use the Linx SDK Interface, you must purchase a FactoryTalk Linx Gateway license.
  • Standard Activation
    Permits communications with a single device at a time.
  • Extended, Distributed, or Professional Activation
    Permits communications to multiple devices simultaneously. The Linx SDK Interface supports up to 200 clients and 200 devices.
For more information about licenses, see Activation types and capabilities in
FactoryTalk Linx Gateway Help
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal