Items on Linx SDK Interface

The following table shows the items on
Linx SDK Interface
.
Items
Descriptions
Activation Status
Shows the status of the FactoryTalk Linx Gateway activations. Refer to Activation types and capabilities in
FactoryTalk Linx Gateway Help
.
Disabled or Enabled
Controls access to the Linx SDK Interface.
Access Control: Specify the clients that can access FactoryTalk Linx SDK
Specifies the clients that can access the SDK API.
  • All
    Grants access to all clients.
  • Listed Client
    Grants access to the clients in the client list. The clients must have digital signatures.
Refresh
Refreshes the client list.
New client requests are listed with the disabled status after refreshing.
Add
Adds a Signer Name of digital signature.
Delete
Deletes the selected clients.
Client
Shows the client's Signer Name that:
  • Requested access to the API.
  • Added to enable or disable access to the API.
Enabled
Defines the API access status of the client.
  • On
    : API access is turned on.
  • Off
    : API access is turned off.
Last Request Time
Shows the time that this client last requested API access.
Ascend icon
Sorts the table's contents in ascending order based on the column's items.
Descend icon
Sort the table's contents in descending order based on the column's items.
Filter icon
Filters the column's item.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal