OPC UA index range

The OPC UA service supports access to array values via index range.
Namespace mode
Index range
Folders with scalar data
Supports the one-dimensional (1D) scalar array. The length limitations of different data types are:
  • BOOL: 3808
  • INT/UINT: 238
  • DINT/UDINT: 119
  • SINT/USINT: 476
  • REAL: 119
Tag list and structures/array access
Supports the one-dimensional (1D) and two-dimensional (2D) scalar array or structure array.
Custom namespace
Supports the one-dimensional (1D) and two-dimensional (2D) scalar array or structure array.
TIP: The Byte array is not supported.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal