Remote Gateway (DA Client remote configuration)

Remote
FactoryTalk Linx Gateway
enables an
OPC
DA client to access a remote
OPC
DA server like
FactoryTalk Linx Gateway
without installing
Rockwell Automation
software on the
OPC
DA client computer. It is intended for use with
OPC
DA clients that do not support server enumeration and cannot discover or identify remote
OPC
DA servers.
During the installation, the Remote
FactoryTalk Linx Gateway
installer configures the
Windows
Firewall and security settings to allow DCOM communications between the
OPC
DA client and Remote
FactoryTalk Linx Gateway
.
Remote Gateway (DA Client remote configuration) does not install services and configures the computers' Windows Firewall settings for an OPC DA client to communicate to FactoryTalk Linx Gateway on a different computer. Select
Remote Gateway (DA Client remote configuration)
to install Remote
FactoryTalk Linx Gateway
. The OPC test client will be installed, and the installer will configure the Windows Firewall settings to allow the opctest.exe and TCP port 135 during installation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal