Where to install Remote Gateway (DA Client remote configuration)
Install Remote Gateway (DA Client remote configuration) on the same computer as an
OPC
DA client that does not support server enumeration.Shown below are multiple
OPC
DA clients connecting to a single FactoryTalk Linx Gateway
OPC
DA server. Remote Gateway (DA Client remote configuration) is installed once per computer that hosts an OPC
DA client.DA Client remote configuration

For more information about DCOM authorization level change, see Application authentication level for DCOM security.
Provide Feedback