Configure Windows firewall for Remote FactoryTalk Linx Gateway
If you install Remote
FactoryTalk Linx Gateway
on a remote third-party OPC client, you
must configure Windows
firewall to allow connections with the FactoryTalk Linx Gateway
server. This is automatically configured after installation of FactoryTalk Gateway
version 3.90.00 and later. If you want to verify the setting or
make changes, follow these steps.To configure Windows firewall
- SelectStart>Control Panel>System and Security(View by: Category).
- In the Windows search box, enterAllow an app through Windows Firewall, and then pressEnter.
- In theAllowed Programs and featureslist, verify theprogramOPCTest.exewhichFactoryTalk Linx Gatewayprovided, or your own application for remote connecting, is in the list. If you cannot find it in the list, you can clickAllow another programto browse and add it to the allowed programs list.
- ClickOKto save the changes and close the dialog box.
Provide Feedback