Create mappings for the signed-in user

To sign in to Historian WebTrend, use a Windows-linked FactoryTalk user account. On the computers with Asset Framework and Data Archive installed, create a security mapping for this user. If multiple users sign in to Historian WebTrend concurrently, you can create a group for these users, and then create a security mapping for this group.
  • To create a security mapping for Asset Framework in System Explorer, see
    Manage mappings in PI AF
    in
    AVEVA-PI-System-Explorer-2024-User-Guide_EN.pdf
    . Find this file in
    C:\Program Files (x86)\Common Files\Rockwell\Help\FactoryTalk Historian SE\Asset Framework
    .
  • To create a security mapping for Data Archive in System Management Tools, see
    Creating security mappings
    in
    hse-in025_-en-e.pd
    f. Find this file in
    C:\Program Files (x86)\Common Files\Rockwell\Help\FactoryTalk Historian SE
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal