Configure Historian WebTrend

If Historian WebTrend is installed on different computers from Asset Framework and Data Archive, you must do the following:
  • Connect to Asset Framework and Data Archive
  • Activate Historian WebTrend
  • Create mappings for the signed-in user
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal