Deleting material classes
- From theMaterial Classesdialog box, select the class, and then clickDelete.
- If theConfirm deletionis enabled on theUser Preferencesdialog box, a confirmation message opens. To delete the class, clickYes.If theConfirm deletionis disabled on theUser Preferencesdialog box, the material class is deleted without a message (see Configuring the Material Editor for more information).IMPORTANT:You cannot delete a material class that is assigned to a material. You must either assign a different material class to the material or delete the material.
Provide Feedback