Engine diagnostics counters
The Engine diagnostics counters are created when the Engine.dll is loaded during startup of the
FactoryTalk Linx
process, and they persist until the process is shut down. They appear on the diagnostics tree as:- Engine
- Transaction Manager
- Connection Manager
The diagnostics counters are:
- Number of transactions in use
- Size of transaction poolTIP:FactoryTalk Diagnostics Counter Monitoris intended for use by qualified Rockwell.
Provide Feedback