Packets (with callback) received
Description
The number of transaction packets that the
Connection Manager
received. This is only applicable for transactions with callback function registering. Provide Feedback