Number of transactions in use

Description
This is the current number of Transaction objects in use, representing the number of currently pending communications requests. It is not unusual for this number to be zero in a lightly loaded system that is experiencing no communications problems. A large number could indicate communications problems (as pending communications requests are in the process of timing out), or it could indicate a backed-up queue, possibly due to a heavily or excessively loaded system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal