FactoryTalk Diagnostics Messages tab

The FactoryTalk Diagnostics Messages tab shows the contents of the FactoryTalk Diagnostics Event viewer on
FactoryTalk Diagnostics Counter Monitor
. This enables you to see whether there is any correlation between the logged messages and the values of the diagnostic items.
TIP:
FactoryTalk® Diagnostics
messages are shown for the local workstation.
DiagnosticsCounterMonitor Linked Icons PNG File Template
This area shows a subset of the entire FactoryTalk Diagnostics message log by default. You can change this view to show all messages setting preferences for the FactoryTalk Diagnostics Messages viewer.
The contents of this tab does not automatically update when FactoryTalk Diagnostics messages are received. To refresh the message log, click
Refresh
on the tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal