Application page (TrendPro)
How do I open the Application page (Properties dialog box)?
- On thePropertiesdialog box, click theGeneraltab.
- ClickApplicationin the left pane.
Application properties allow you to create customized trends that emphasize important data effectively. The following properties are applied immediately to the current trend.
The following options are available:
Properties | Description |
|---|---|
Line styles | The color, format style, and weight of trace lines in the chart. The number of the trace corresponds to the trace order as it is displayed in the Trace List below the plot surface. Click anywhere in the line style to change it. |
Highlighted | Adjusts the color, format, and line weight of a highlighted trace. |
Trace dimming | The brightness for traces that do not have focus when multiple time periods are used. |
Provide Feedback