Chart page (TrendPro)
How do I open the Chart
page (Properties dialog box)?
- On thePropertiesdialog box, click theGeneraltab.
- ClickChartin the left pane.
Chart properties allow you to set the title, information that displays in tooltips, zoom, and other options that display in the current
trend. The following properties are applied immediately to the current trend.The following options are available:
Property | Description |
|---|---|
Title | The title to use. Select one of the following options:
You can set the title's font, style, size, and effects by clicking Font . |
Margins | The amount of white space on the plot surface (in pixels). |
Tooltips | Select the content of the tooltip from the following options:
|
Zoom and Pan | The display of the plot surface. Select from the following options:
|
Automatic scaling | Determines the method used to automatically scale data based on the following:
|
Background | Determines the background color or image. Select from the following options:
|
Cursors | Determines how the cursors display data when enabled. Select from the following options:
|
Trace layout | Displays each trace in its own grid or zone.
|
Annotations | Once enabled, it allows you to view, add, edit, or delete annotations for the FactoryTalk Historian SE trace from the runtime context menu. Note: To view all the annotations, choose the raw retrieval mode via General > Retrieval > Raw . The other retrieval modes (automatic or custom) filter tags, thus not all the annotations will show on the trend. |
Provide Feedback