Highlight the active trace (TrendPro)
Highlight the currently selected tag
on the plot surface to make it easier to see when you have multiple tags on the plot surface.
To highlight the active trace
- On theTrace List, select the trace you want to highlight.
- On the toolbar, clickTrace Highlighting
.The trace you selected is highlighted on the plot surface.
Provide Feedback