Data Grid Properties dialog box
Use the dialog box to configure general settings for the data grid object. The following table shows options on the
Genera
l tab.Option | Description |
|---|---|
Setup | Select to open the Properties dialog box where you configure the detailed data binding and appearance at runtime.The Properties dialog box is also available at runtime if you select the Properties runtime option. |
Runtime options | Select which shortcut menus are available to operators at runtime.
|
Provide Feedback