Data Grid Setup Properties - Appearance tab
The following table shows options on the tab.
Option | Description |
|---|---|
Show columns | Indicates the number of columns to be shown on the data grid object. |
Column | Shows the name of the selected column. Clear the check box before a column to hide it. |
Header | Enter the header name of the column. |
Decimal places | Specify the number of digits after the decimal separator. |
Width option | Select an option that determines the automatic sizing mode for the column.
|
Width | Enter a value to specify the column width in pixels. |
![]() | Select to move the column up. |
![]() | Select to move the column down. |
Headers | Select to configure the font styles for headers. |
Cells | Select to configure the font styles for cells. |
Banded row | Select to configure the shading color for alternate rows. |
Gridlines | Select to configure the grid line color. |
Header row height | Select Auto to automatically adjust the height of header row. Clear Auto to enter a value for height in pixel. |
Row height | Select Auto to automatically adjust the height of body rows. Clear Auto to enter a value for height in pixel. |
Provide Feedback