Data Grid Setup Properties - Data Binding tab
The options vary depending on the selected data source,
SQL Server
, Data Log
, or FactoryTalk Historian
. Only one data source's configuration can be saved. Switching to another data source will clear the current data source's configuration.The following table shows options on the tab if
SQL Server
is selected as the data source.Option | Description |
|---|---|
Choose table/view | Displays the available tables and views of SQL Server database. Tip : In the search box, enter text to quickly filter the column names. |
![]() | Adds the selected column to the data grid object. Use the Shift or Ctrl key to select multiple columns. |
![]() | Adds all columns of the selected table or view to the data grid object. |
![]() | Removes the selected columns from the data grid object. Use the Shift or Ctrl key to select multiple columns. |
Column | Shows the name of the selected column. |
Type | Shows the data type of the selected column. Tip : The following column types are not supported: hierarchy, geography, and geometry. |
Filter | Double-click the cell to create a filter of the selected column. If the data type is datetime , datetime2 , smalldatetime , date , or time , you can select Set as time period on toolbar to show it on the toolbar and dynamically set the time period at runtime.Only the records that meet the filter criteria are displayed on the data grid object. Tip : To filter cells with empty values, use Equals '' . Data types text and ntext don't support Equals or Not equal to filters in SQL Server databases. |
Sort | Sorts the selected column. You can apply multiple sorting orders at the same time. A number is displayed besides the sorting order and indicates the sorting level. Sort precedence is determined by the sorting level. For example, if you want to sort by Severity and then TicksTimeStamp , apply the first sort to Severity and the second sort to TicksTimeStamp.Select X to remove the sorting. |
Maximum rows to show | Configures the maximum rows to show on the data grid object. The maximum capacity is 50,000. |
Use the local machine time zone | Shows the time and date according to the time zone of your local computer. Tip : It's recommended to select this check box when datetime , datetime2 , and smalldatetime data types are logged as Coordinated Universal Time (UTC) in the database. |
The following table shows options on the tab if
Data Log
or FactoryTalk Historian
is selected as the data source.To show data log logged to a remote computer, Change the logon account of Datalog ReadEx Service.
To show historical data of FactoryTalk Historian, you need to install
FactoryTalk Historian Connectivity
from the FactoryTalk View installation package on the FactoryTalk View Studio or SE Client computer. For more information, see PI SDK Utility Help.Option | Description |
|---|---|
Choose (Historian) tags | Depending on the selected data source, it displays the available tags of data log models, DataLogPro, or the FactoryTalk Historian SE server. Tip :
|
![]() | Adds the selected tag to the data grid object. Use the Shift or Ctrl key to select multiple tags. |
![]() | Adds all tags to the data grid object. |
![]() | Removes the selected tags from the data grid object. Use the Shift or Ctrl key to select multiple tags. |
Tag Name | Shows the name of the selected tag. |
(Data) Type | Shows the data type for a tag. If the data source is data log model, the options are Numeric or String . Select the correct data type of a tag for it to show on the data grid object. |
Filter | Double-click the cell to create a filter of the selected tag value. Only the records that meet the filter criteria are displayed on the data grid object. Tip :
|
Sort | Sorts the selected tag values. You can apply multiple sorting orders at the same time. A number is displayed besides the sorting order and indicates the sorting level. Sort precedence is determined by the sorting level. For example, if you want to sort by Tag1 and then Tag2 , apply the first sort to Tag1 and the second sort to Tag2.Select X to remove the sorting. |
Time period | Sets the time period for when the tags are recorded. The object will show the tags recorded during that period. |
Sort | Sorts the overall tag values by time in the ascending or descending order. |
Interpolated mode (applicable to FactoryTalk Historian only) | Shows the interpolated data generated at a certain time interval. During the historical data querying, there may be intervals with no raw data in the database. Rather than values from actual historical records, interpolated values are mathematically interpolated at a given interval, and thus not actual archived data. |
Limit number of records returned to / Maximum rows to show | Configures the maximum number of records returned by the data log or historian server. After being filtered and sorted, the records shown on the data grid will be less than or equal to the configured number. The maximum capacity is 50,000. |
Provide Feedback